We are using an nrf52 base to communicate to the ADS1299-4 and on powerup we are seeing DRDY constantly pulled high. I`ve followed the startup sequence detailed in the data sheet and am still seeing no effect on the DRDY pin. Pulling START pin low and PWDN pin low also have no impact on DRDY state. The SDATAC command also has no impact.
SPI Library works as expected and SCLK/MOSI pins are working as expected. The frequency we are running at is 2MHz. This behaviour is happening on two different boards constructed using the diagrams and layouts detailed on the data sheet for bipolar operation.
Any help is appreciated.