This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DLP2010LC: Which chip, old DLP2010 or new DLP2010LC will be installed on the DLP2010EVM-LC board?

Part Number: DLP2010LC
Other Parts Discussed in Thread: DLP2010,

Hello!

When purchasing a DLP2010EVM-LC evaluation board from ti.com/store, which chip will be installed on the board of the old DLP2010 or the new DLP2010LC?

The post e2e.ti.com/.../faq-new-dmd-part-number-for-dlpc347x new chips with new firmware.

Zhukov Vladimir
  • Hello Vladmir,

    It depends on the build date of the EVM. The newly manufactured EVMs will have the DLP2010LC DMD. In case the optical engine of  the EVM was manufactured prior to introduction date  then it will prious version of the DMD.

    regards,

    Vivek