This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi E2E support,
I would like to ask about pattern sequence configuration for DLP4710/DLPC3479.
My customer wants to project the second and the subsequent patterns without any commands.
In other words, they want to project multiple patterns by using a pulse.
[Background]
Now, they are using DLP4500/DLPC350, and they are configuring the sequence described in an attached file.
They want to replace to DLP4710/DLPC3479.
Would you please tell me the above pattern sequences can be realized.
If yes, would you please how to set on GUI tool.
Best Regards,
Koike
Hello Koike,
Thank you for your query, the DLPC3479 does support this feature. you are asking about "trigger in" I recommend you read about Internal pattern mode in the DLPC3479 datasheet.
Regards,
Arthur Brown
Hello Arthur Brown,
Thank you for your answer.
According to "Figure 23 Trigger In Mode" in DLPC3479 datasheet, Trigger In signals(External) need to be input continuously to project each pattern.
We want to project multiple patterns by using "One Shot" Trigger Input pulse.
According to DLPC3479 Software Programmer's Guide, there is the following description.
=====
3.5.1.1 Write Parameters (90h)
The controller uses Trigger In Enable to indicate in which Internal Pattern Streaming mode the system operates:
=====
Best Regards,
Koike
Koike,
As I understand the trigger input is required to "trigger" each pattern sequence if this function is enabled. If you don't want to wait for a trigger input, you can simply disable the "Trigger In Enable" per the DLPC3479 Programmer's Guide. The entire pattern set will play when you start the sequence.
Are you having any issues with this feature? Let us know if that is the case.
Regards,
Philippe