This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi TI's Gays
I am a system engineer from Wintech which is TI' important third party
https://www.wintechdigital.com/PRO4710
We have developed several products using TI's DLPC3479
Now we are developing new DLPC3479 device for AOI and SPI
Our 3D AOI device uses 4 DLPC3479 optical engines installed in four directions, for example represented by A-B-C-D
Four devices are working at internal pattern mode and free running mode
Each device will play once if geting start control command,for example W 36 9E 00 00, from IIC control interface
Four Trigger out2 signals, output from each device, are connected together to trigger camera
Four DLPC3749 devices project pattern image in turn, For example first from A to second B to third C to last D
So I run into a difficult problem , When should the next device be notified if the current device completes the patterns
I add a MSP430 into the hardware system and MCU can send DLPC3479 command from IIC interface
Also, I have connected both four DLPC3479 Trigger Out1 signals and Trigger Out2 to MCU GPIOs
What I want to know:
How can I change the function of Trigger Out1, to the status of completed patterns projection from the begining of the pattern set
Or
How can I add another Trigger Out3, which will be sent out when all the patterns are projected
The "TIRef-DLPC3479-DLPA3005-AC_Only-CurrentLimitsRemoved-BlueOnly-v8p1p001" and "TIRef-DLPC3479-DLPA3005-TIEVM-CurrentLimitsRemoved-v8p2p0"
DLPC3479 composer projects zipped files were shared with me from Austin Snyder and Arthur Brown
Could you share me app347x_dual_v4.4.0.bin file all-in-one source and I can modify the source code by myself
PS:
I have experience in modifying DLPC442x all-in-one source code, I think I have the ability to modify the API sound code of DLPC3479
Thank you very much
Best Regards
Jia
Hello User,
Please allow us some time to look into your request and come back to you next week.
Regards,
John
Hello Jia,
Our expert will get back to by mid of this week via email.
Thanks for your patience
Regards,
Akhil
Hello Akhil
Thank you very much for your help
waiting for good news
Best Regards
Jia
Hello Jia,
Since this question is being addressed off of the E2E forum, I will be closing this thread. Please feel free to reply to this or re-open the thread.
Regards,
Austin