Dear All,
As we know,"Maximum power can also depend on how well optimized the calibration routine was and the calibration data that was flashed onto the system. "
I want to know how to optimize the calibration routine and the calibration data that was flashed onto the system?
Parameters in the picture:(The power is 3W(current:0.25A voltage:12V))
LDC Index=0;
Red:35173;
Green:50284;
Blue:38829;
Current Limit:59000;
Thanks,
Mr. Wang