HI,
I want download DLPC120 Control Program ,but i can just find the DLPC120 Automotive Control Program Lite 1.3.1.41.
Where can i get the full version of DLPC120 ACP?
Thanks!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
HI,
I want download DLPC120 Control Program ,but i can just find the DLPC120 Automotive Control Program Lite 1.3.1.41.
Where can i get the full version of DLPC120 ACP?
Thanks!
Hi,
Welcome to the E2E forums and thank you for your question.
Please provide a valid email and make sure you have a TI account created and I can share you the download links to the full version of the DLPC120 Automotive Control Program.
Thanks,
Alex Chan
Hi,
Please also ensure you have a myTI account so I can grant you access.
Thanks,
Alex Chan
Hi,
Just granted access. Please wait a little and you should get an email notification. Let me know if you do not get it.
Thanks,
Alex Chan
Hi
I get the email and setup the DLPC 120 ACP .
I am confused which one of Piccolo application software should i download,maybe this page is wrong?
By the way,I used DLPC230 ACP to calibrate RGB,it work with DLP composer.Whether there is a matching calibration software for DLPC120 such as DLP composer?
My leader have a DLPC120 EVM,and I use the DLP120 PCBA developed by my company, Is there any difference in the software requirements for calibration?
Thank you
Hi,
I have attached a DLPC120 ACP user guide for reference as well as a guide on calibration.
7026.DLPU059_ACP_UsersGuide_March2018 (2).pdf
5226.DLPU066_Calibration_User_Guide_March2018 (3).pdf
The HUD Piccolo SW release contains Piccolo main application code in case a user may be programming a blank Piccolo MCU.
The HUD Piccolo bootloader SW release contains Piccolo bootloader code in case a user may be programming a blank Piccolo MCU.
You can read more about the use for those two folders in the user guide in section 5 about reprogramming the EVM. If you acquired a TI EVM it should already come default with the bootloader and main application already programmed.
The EVM Rev C starter cal folder is useful starting point to get going with the calibration routine and please see more information in the calibration user guide.
Unfortunately there is no open customer available DLP Composer tool like for the DLPC230 ACP and .55 chipset. There is an internal DLP Composer tool for TI engineering only use but if you require a different configuration file I can create a build for you with the specific features or settings you may be looking for.
Hope this helps.
Thanks,
Alex Chan
HI
Thank you for your patience.
I understand the flash and calibration process.
Thanks