Other Parts Discussed in Thread: DLPLCRC410EVM, DLPLCR95EVM, DLPLCR65EVM, DLPC900, DLPLCRC900EVM
Hello,
I am a postgraduate, I'm hoping to use DMD as a controllable "pinhole array" in a confocal measurement system, as a subsitute for area-scan. Instead of projection lens, I will use a objective lens to focus the light reflected from the ON pixels to the sample. The basic structure is similar to the picture, also similar to a light-field camera.
I'm having some confuse choosing the DMD, especially the DLP engine. For example, what is the difference between "DLP LightCrafter 6500 EVM" and "DLP 9500"?
With respect to the patterns on DMD, the detection of corresponding pattern on the CCD is a major problem for me, can you recommend a DLP that can realize my design purpose?
Also, are there any documents offering reference to the system optical design?
Thank you in advance!