This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Scenario | Error details | Remediation steps |
Invalid Material | Fullscreen 1 2 3 4 5 6 7 8 9 10 11 12 13 14 15 16 17 18 "errors": [ { "errorCode": "ERR-TICOM-ORDER-API-0002", "type": "Application", "section": "lineItems", "field": null, "reason": "Invalid Part Number", "message": "Resubmit order with correct TI Part Number", "data": [ { "customerLineItemNumber": "1", "tiPartNumber": "SN74LVTH163", "quantity": "1000", "availableQuantity": null } ] } ] XXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXX "errors": [ { "errorCode": "ERR-TICOM-ORDER-API-0002", "type": "Application", "section": "lineItems", "field": null, "reason": "Invalid Part Number", "message": "Resubmit order with correct TI Part Number", "data": [ { "customerLineItemNumber": "1", "tiPartNumber": "SN74LVTH163", "quantity": "1000", "availableQuantity": null } ] } ] |
The material you entered is not an orderable part number. TI.com search can suggest the closest match to your part number. |
**Attention** This is a public forum