Dear Samip and team,
Can I order multiple part number under one order API sending ? It turns that if one line items is falling (quantities requested is above availability or other issue) then the return Jason is NULL/Empty and so is the status of the specific Line items.
Why is this behavior in API 2 ? The return status in the Json that is received should contains status and not empty even if one of the items was not successful.
Please advice if not clear, and if clear please advice how to order multiple orderable part numbers and still get the correct status for each line item.
Please also advice what are the possible return statuses for ORDER API. Up until now we only see PROCESSSING or (empty)
Thanks in advance.