This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
today we had two orders (T04800582, T04800590) canceled shortly after ordering with the order status Payment rejected. But in the list of confirmed payments on Apruve, both are there in the status accepted.
In addition, these two orders are not visible in the Order history on the TI website.
Orders can be seen through the api, but their items do not have a set status.
{ "tiLineItemNumber": "1", "customerLineItemNumber": "3", "tiPartNumber": "SN74CB3T3245DGVR", "tiPartDescription": "3.3-V, 1:1 (SPST), 8-channel FET bus switch with level shifter", "customerPartNumber": "SN74CB3T3245DGV", "customReelIndicator": false, "partType": "IC", "eccn": "EAR99", "quantity": 250, "shippedQuantity": 0, "unitPrice": 0.839, "netPrice": 209.75, "packageInformation": { "carrier": "LARGE T&R", "delivery": [ { "type": "Cut tape" } ] }, "waiverAvailable": false, "trackingAndShipping": { "creditMemo": [], "invoices": [], "trackingNumbers": [] }, "customerReferenceNum": "SN74CB3T3245DGV" }
On Apruve, other canceled orders from this year also reduce our credit there. Total 8 orders in 2024.
Petr,
We will continue to correspond via the private chat. Thanks!!
Regards,
Faye
Hi Petr,
Per our conversation, we've addressed this issue and you should not see a problem now. I'll move forward with closing this thread. Thanks for your patience!
Regards,
Faye
Hi Faye,
From our side, we keep seeing the same problem.
Today we have 2 more orders cancelled by PAYMENT REJECTED - T04810611 and T04809715.
Still the item returns no status in json.
Orders still not visible in history on TI website.
Edit:After two more canceled orders, today's fifth was confirmed. They all had the same item in the same quantity.
T04810611 | Payment rejected |
T04809715 | Payment rejected |
T04809722 | Payment rejected |
T04810640 | Payment rejected |
T04807703 | Complete |
Petr,
Sorry you are still experiencing some issues. Let me raise this again so that our team can investigate. I'll provide an update on tomorrow.
Regards,
Faye
**Attention** This is a public forum