Part Number: TCA6424A
Other Parts Discussed in Thread: TCA6424
Hi Team,
In data sheet, it is necessary to set all IOs as inputs to achieve lower power consumption. Is there any other way to make IOs not need to be set as inputs to achieve lower power consumption? Or some ports keep the output high, and other ports are set as input, can the power consumption be reduced?


TCA6424ARGJR's IO is all used as output GPIO application (output high or output low) in normal working mode,
Some modules cannot be powered down when the system is in sleep mode, and their power is controlled by the IO of TCA6424ARGJR, so the output is high even in sleep mode;
The whole system has low power consumption requirements, and it is not possible to set all the IOs of TCA6424ARGJR as inputs to reduce its power consumption, so customer would like to confirm whether there are other ways to make all or part of the IOs of TCA6424ARGJR can be set as output and function. Consumption is reduced to a minimum;