Part Number: AM26C31
Hi,
- We are using AM26C31 part for our applications. We use baud rate of 115200. In datasheet,there is a graph detailing about switching frequency vs supply current. From the graph,it is noted that for 115200,supply current will be 120mA when all the four channels are operating simultaneously. So power dissipation in IC will be 120mA*5V = 0.6W. Is this correct whether IC will consume 120mA for 115200 baudrate? Also please clarify whether any other power dissipation factor also to be considered or only 0.6W dissipation.