This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DP83869HM: DP83869HM Current consumption per rail in two supply mode

Part Number: DP83869HM


DP83869HMRGZT is operated in Two-Supply Mode, SGMII to Copper 1G, cable length <10m, Max temperature - 75 deg C

VDDIO = 3.3V

VDD1P1 = 1.1V

VDDA1P8= NC

VDDA2P5 = 2.5V

In other forum links I could find current consumption in three supply mode only. Please provide the current consumption detail on each rail for the above configuration and operation.