Part Number: TRS3223E
Hi,
For TRS3223E only used one DRIVER and RECEIVER.
Can be the second DRIVER/RECEIVER(pin8,9,10,12) floating? thanks.

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Rock,
The digital input pins (Din pin 12) should always be tied to a known voltage. This can be tied directly to Vcc or GND.
The Rin pins (pin 9) are designed to deal with a high-z case so these can be left floating. All output pins may also be left floating (pins 8, 10).
Let me know if you have any more qustions.
Regards,
Eric Schott