Hello,
I have a couple of 7.2Gbps aggregated data streams sent out at TLK10022 HSTX_A/B_P/N outputs and received by Xilinx FPGA at MGTHRXP/N inputs.
Regarding the FPGA RXDATA CLK one option is to use the recovered CLK from the RXDATA inside the FPGA and another would be to feed an RXCLK as the REF CLK to the FPGA to have a better RX CLK quality especially from jitter stand point.
I am using a single REF CLK to drive both TLK10022 A/B channels and use only the aggregator portion of TLK10022 (TX side).
TLK10022 has CLKOUT_A/B_P/N outputs and according to the datasheet it could be driven by HS_RXBCLK_A/B (not used in my case) or VCO_CLK_A/B_DIV2.
Q1) VCO_CLK_A/B_DIV2 and its relation with HSTXA/B_P/N output data stream at 7.2Gbps, regarding the frequency, delay between CLK/DATA, etc.
Q2) Since I don't use the HSRX_A/B_P/N RX side what is the TI recommendation for the unused RX CML inputs and overall RX section?
Regards,
Reza