Part Number: DP83822I
Other Parts Discussed in Thread: TIDA-00928
Hi team,
My customer is tesing DP83822I in a low temperature test. DP83822I is configured into RMII master MODE. They put the board in -40℃ for several hours and then power up the board. The result is some DP83822I boards can work normally but some cannot bulid up link with the partner after power up. The failure rate is 3 out of 10. For the failure devices that cannot bulid up link, we found that their Pin1 have no signal at all. But in theory, Pin1 should have a 50MHz clk output in RMII master mode. So could you please help advise what may cause this issue?
What's more, for the failure devices, we tried to disconnect the CRS_DV line from DP83822I to MAC. Then all the failure devices can build up link after start up in low temperature. So why CRS_DV line makes a difference here? Can we just leave this pin open in RMII master mode? Thanks.
Best regards,
Wayne