Part Number: TPS65987D
Hi team,
Is the current limit applied when the LDO_3V3pin(9pin) and 1V8pin(35pin) are short to GND?
Sincerely.
Kengo.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Kengo,
There is no active current limit on the LDO_3V3 and LDO_1V8.
If either pin is shorted to ground, it is likely to damage the device.
The LDO_1V8 is used as the main digital power supply, so the device will brown out with any external load applied to it.
The LDO_3V3 is intended for very limited external use. It will run out of power at about 10mA of load.
Regard,s
Chuck