Other Parts Discussed in Thread: TPS54325
Regarding this intermittent issue with some SN75DP130 devices not always detecting a DP monitor asserting HPD_SINK high before the SN75DP130 +3.3v power is stable because flip flops inside the DP130 HPD controller can initialize to a wrong state -
Is there a possible software work around solution for this issue? The DP130 data sheet indicates that by default, it automatically goes into Standby mode to conserve power if the HPD_SNK signal goes low for longer than 2 msec. So does this intermittent issue with the HPD controller flip-flops initializing to the wrong state only occur when the DP130 is in the Standby mode? Or can incorrect HPD controller flip-flop initialization also occur in the non-Standby modes as well? We would pursue disabling Standby mode (by setting AUTO_POWERDOWN_DISABLE in I2C Control Register offset 01h to a "1") if that will prevent this issue of the DP130 not always detecting the powered up monitor asserting the HPD_SNK signal high. Thanks.