Part Number: TCA9545A
Dear Team,
When using the TCA9545A as a level shifter at the same time, if the signal input criterion conflicts with 0.7VCC, how to understand the relationship between Vdpum and Vdpux? Can the former be smaller than the latter? Thanks!
For example, VCC=2.5V, Vdpum=1.8V, Vdpux=3.3V, is the usage restriction required that VCC must be equal to Vdpum, and then Vdpux is greater than Vpass

Many Thanks,
Jimmy