Part Number: FPC402EVM
Other Parts Discussed in Thread: FPC401, FPC402
|
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: FPC402EVM
Other Parts Discussed in Thread: FPC401, FPC402
|
Thanks Nasser , for the Response,
i send friend Request please do needful , here i am sharing my mail id :- hramala@qti.qualcomm.com.
i got setup_FPC401_EVM.exe installer , i successfully create the link , but i am not able to read and write the Local instance & downstream i2c registers , can you share me the setup_FPC401_EVM_with_RTE.exe also .
I fallowed programmers guide to reset FPC (resetting the fpc default address) , i2cset -y 1 0x0f 0x00 0x8F (Updating the register offset 0x00 with 0x8F
) but still FPC was responding to programed address, does i need to any additional stuff apart from this ?
Thanks,
R. Harshavardhan.
Hi Ramala,
You now have access to the FPC402 design files including GUI, SDK, and the programming guide. Within 20-30 minutes you should be able to access these files.
Regards,Nasser
Hi Nasser ,
yes i tried the procedure which mentioned in the programming guide , when i reset the FPC through Registers All the register values are going back to the default reset values , but FPC was failed to Reset its i2c address ,
i2cset -y 1 0x0f 0x01 0x18 (updating I2C Device ID Register 0x01 with 0x18 )
and FPC-i2c address is still the configured i2c address (0x0c = (0x0x18 >> 1).
default i2c address.
In shot we are setting the Reset-Register with 0x8F and then 0x0 for reset the fpc, but still fpc i2c address failed to reset to the default value.
Greetings,
Please note default I2C address is 0x1E not 0x1F.
Additionally valid I2C 8-bit addresses are listed in table 6 of the FPC402 data sheet.
Regards,,Nasser
sorry typo mistake , default address was 0x1E only , i am fallowing the the table 6 of the FPC402 data sheet ,
and, I am programming the i2c address of FPC with 0x10, and i able see the 7 bit address of all FPC (0x08), QSFP-0 (0x40),
QSFP-1 (0x42) .
in my Exit Routine of the driver i am resetting the FPC , so that the Register address 0x01 was becoming 0x3F(default value),
but the FPC i2c-adress was still (0x08 = programmed address), ideally after reset is should be (0x0f default 7 bit address) = 0x1E.
Fallowing below reset sequence :-
setting the Register offset 0x00 with 0x8F and then 0x0
i2cset -y 1 0x08 0x00 0x8F
i2cset -y 1 0x08 0x00 0x0
Hi Ramala,
Valid FPC addresses are listed in table 6. If you change I2C addresses it should be one of the addresses noted in this table.
Regards,Nasser
hi Nasser,
yes i am programming the FPC i2c address with one of the i2c address mentioned in table 8-6 .
By default FPC i2c address was 0x1E and corresponding i2cdump was

I am programming the fpc with address in table 8-6 for fpc instance - 10

write 0x18 to fpc register 0x01
i2cset -y 1 0x0f 0x01 0x18 and Dump was

Fallowing below sequence to reset fpc :-
setting the Register offset 0x00 with 0x8F and then 0x0
i2cset -y 1 0x08 0x00 0x8F
i2cset -y 1 0x08 0x00 0x00

Here the Issue not with default i2c address nor with the setting i2c address of FPC , i am fallowing table only , issue with i2caddress was not reverting back to its default value ie 0x1E, Even after Reset of FPC using register offset 0x00.
Hi Ramala,
Please write 0x0F into reset register offset 0x00. Do you see I2C addresses restored back to the table 6 settings?
Regards,Nasser

yes Even after writing 0x0F to the reset register offset 0x00 was failed to restore I2C addresses back to the table 6 setting ie default address 0x0E .
Hi Ramala,
It seems the only way to restore the registers back to the default setting is to write 0x8F into reg 0x00. Since this works, what prevents you from writing 0x8F into reg 0x00? We don't see an issue using this workaround.
Regards,Nasser
Hi Nasset,
can you check my previous comments , i Explained how i am Resetting the FPC , i tried writing 0x8F to offset register 0x00 , Even after FPC was responding to programmed i2c address only , not the default i2c address 0x1E, after resetting the the offset register 0x01 going back to default value 0x3F but still FPC failed to Respond to its default address, can you please check my pervious comments i explained very clearly there .
is there a possibility to toggling the EN pin through software ? that might solve my problem .
Thanks,
R. Harsha
Hi Ramal,
I re-read your earlier comments and i had mis-understood your earlier statement. If i understand this correctly you have:
Reg 0x00 = 0x8F
Reg 0x01 = 0x3F
However, even though reg 0x01[0]=1'b1 device is not going back to the default 0x1E default address setting. I am assuming this device has SET_ADDR_N(CTRL3) tied to GND. Please confirm.
Regards,Nasser
Yes, ADDR_N(CTRL_3) tied to GND with the help of Jumper cable provided along with Evolution board.
toggling the EN pin means EN = GND and then EN = VDD1 I was able to reset the FPC i2c address to its default address 0x1E.
is there a possibility to toggling the EN pin through software ?
Checked the register map and am not able to find a way to do the same functionality as EN pin. We are continuing to check.
I did one experiment as follows:
1). Power up the device
2). Change reg 0x01 from 0x3F to 0x18 - as you had done.
3). Set reg 0x00 = 0x80
4). Readback reg 0x01 and i see default value(0x3F).
Can you please follow these exact steps to see if you can duplicate my finding.
Regards,Nasser