This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS65987DDK: Is there a wide temperature product of -40 ℃ ~85 ℃ that supports 100W power source

Part Number: TPS65987DDK
Other Parts Discussed in Thread: TPS65987D, TPS55288, LM3489, LM5175, PMP20042, LM61460, LM61440

hi TI

    The customer needs to make the source end, battery powered, 24V input, and 100W output power to charge the mobile phone. There is no data communication demand. Is there a chip that meets the wide temperature(-40 ℃ ~85 ℃) version and can be provided according to the overall design scheme?

I found only 6 chips meeting 100W power, all of which are -10~75 ℃。