I have a client design using the TMUXHS4212RKSR part for routing PCIe to different slots on a PCB. Recently we’ve had some issues where this chip will burn out during use. It doesn’t seem to occur during power cycling but during a longer term test (overnight). The symptoms are a dead chip that won’t pass signals and some burnt traces at Pin 6 (VCC). We did note that the datasheet for the TMUXHS4212 just updated in May 2022 to require the RSVD pins to be connected to VCC instead of allowing floating as an option. We designed this in 2021 and followed the initial recommendation of floating the pins like the evaluation kit schematic does. Could the floating pins be causing the burnout issue? What are the RSVD pins doing and why the recent change?
My other thought is some kind of un expected backpowering, but the chips appear stable through power up.
Best regards,
Travis