In the test process, we found that only analog signals can be used for communication when ISP devices are connected to DS90UB936, which needs to be adapted to the extinction area. And after running for a period of time, there will be a slow downward rotation of the whole picture. we used 25MHz crystal clock and the ISP device model is FH8322, uses MIPI CSI communication, and interfaces are PIN11 to PIN14 of DS90UB936.
Is it possible to fine-tune the frequency of HSTXDBR Data bit rate (about 936Mbps) from the software aspect to adapt to the back-end ISP device?
We have found Indirect Address Page 0x00 at Register 0x40 to 0x48 seems like the register we wanted, but we didn`t find out from the datasheet that how these registers correspond to field synchronization, line synchronization, or extinction zones, and how much time/frequency each unit represents.