Part Number: HD3SS3202
Hi Team,
My customer is asking to confirm whether we have USB-IF certification or compliance test result with HD3SS3202 EVM.
Could you please help to confirm? Thanks.
Terry
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Terry:
we should tested compliance before. but it's pretty old and can't find where it was located. But it should pass USB3 compliance before release it.
Regards
Brian
Hi Brain,
Thanks for your reply.
My customer has an USB communication issue in their product.
While 5G wireless communication is processing, USB communication "ss.inactive" error occurred.
They doubt the issue is related to USB signal loss by MUX HD3SS3202. That's why they asked for our USB compliance test result.
BTW, I have asked customer to send me schematic and PCB to review.
Do you have any advise or checklist regarding schematic and PCB review. Or any other comment for this issue.
Thanks and regards.
Terry
Hi Brain,
One more question.
In HD3SS3202 datasheet chapter 9.2.1.2 Detailed Design Procedure has description below:
The device can support 1 to 2 inches of board trace and a connector on either end.
What exactly is the trace mean?
My customer's whole trace route is CPU-MUX-USB connector-Fan IC.
1 to 2 inches refer to the whole trace? or a specific portion?
Thanks and regards
Terry
PCB trace is a copper conductor on the PCB that conducts signals on the surface of the PCB. how long is trace length on their board?
Are they running 5Gbps or 10Gbps.
regards
Brian
Hi Brian,
They are running 5Gbps. Do you have guidance with trace length?
In my customer application, their trace route is CPU(host)-MUX(HD3SS3202)-Connector-Fan IC(device).
Do you have suggestion about the trace length for each portion? Such as the length between CPU and MUX, MUX and connector...
Thanks.
Terry
Is it type-C application?
so it only allow 6.5db loss on host device side. Hd3SS3202 has -1.3db loss at 2.5Ghz.
so you only have 6.5-1.3=5.2 db loss from CPU to connector (include connector loss). about 10 in trace length
Regards
Brian
Hi Brian,
Thanks for your Patience. Yes, it is type-C.
And let me confirm the trace length again. You mean 10 inch from CPU to connector, right?
I am a little confused cause in the datasheet of HD3SS3202 page14, it has a description "The device can support 1 to 2 inches of board trace and a connector on either end." I am curious 1 to 2 inches here means which portion of the board trace.
Best regards
Terry
yes, 10in from CPU to connector.
in datasheet, it means from 3202 to SOC or connector. 1-2in could be for 10Gbps.
3202 loss at 5Ghz is 2.4db

so at 10Gbps, 8.5-2.4=6db allowed, around 6in trace length from CPU to connector,
3in before and after 3202..