Part Number: DP83822I
Other Parts Discussed in Thread: DP83822EVM, DP83869HM
Hi
The customer has an EtherCAT product, the structure is the EtherCAT Slave IC connected to the DP83822i through the MII interface, and the DP83822i was set to the optical fiber mode through the hardware Strap setting, and the connection can be normally connected through the optical fiber;
However, due to the flexibility of the design, it is necessary to test to set the DP83822i to the copper cable mode, and then connect the fiber module SPS-3120G through RXD_N, RXD_P, TXD_N, TXD_P. Please refer to page 4 of the attached file for the connection method. , Read Bit 14 of 0x000A Control Register #2 (CR2) to confirm that it has switched to copper mode, and the fiber module SPS-3120G also confirms that it can be connected to the fiber hub (the FP LED of the fiber hub is on), the DP83822i’s The CRS STRAP Mode is Mode 4, but the LED_0 maintains the level of about 3V, and the TXD_N and TXD_P do not send any signals. Is there any possible reason why the DP83822i cannot be connected normally?