This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLK10022: How to set register to achieve input in LS and output in LS without via HS

Part Number: TLK10022

Hi team,

     support need!

    The customer finds that there is a path inputting in LS and outputting from LS drawn in green path. So customer wonders to know how to set register to achieve input in LS and output in LS without via HS.

YOURS 

NAN

  • Hi Nan,

    Please try the following procedure.

    1) On LS_SERDES_CONTROL_3, set bits 2 and 3.  Do this for all lanes where you would like local loopback.

    2) On HS_TP_CONTROL, try setting bits 3:0 to either 0100 or 1100.  I think one of these should enable local loopback, although it's not clear which based on the register map description.

    Thanks,

    Drew