This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLK10031: Lane alignment is not achieved on the LS side

Part Number: TLK10031
Other Parts Discussed in Thread: TLK10232

 TLK10031_LS.pdf

our system is as attachment pdf. our TLK10031 config is as follows:

global reset"

"0x8610" > "0x401E0000"

#disable auto-negotiation

"0x2000" >"0x40070000"

#turn off lt_training

"0x0" > "0x401E0096"

#link setting configured manually

"0x03FF" > "0x401E8020“


#HS_SERDES_CONTROL_2

"0x4848" > "0x401E0003"


#HS_SERDES_CONTROL_3
"0xD500" > "0x401E0004"

#data path reset
"0x0008"  > "0x401E000E"

frist seconds ,  CHANNEL_STATUS_1 is 0x1c03 , the but, after a while,the register CHANNEL_STATUS_1 is changed to 0x5c03 .which means Lane alignment is not achieved on the LS side

can you give me the reason for it ?? thanks