This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Product will support USB-PD at bus voltages of 5V and 9V. BQ24392 will be exposed to 9V VBUS for extended (non-transient) time.
The BQ part is only needed to detect legacy chargers, it does not need to operate normally with 9V VBUS.
Will this part survive extended periods with 9V VBUS? The CHG_DET will be clamped to 7V during this time, or will it be Hi-Z?
(I did see the linked thread, but it does not quite answer my first question)
Thank you
This device can tolerant 28V Vbus, so 9v should be fine.
Regards
brian