Hi,
What is the maximum insertion loss that SN75DPHY440SS can support?
Best regards,
Randy
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
What is the maximum insertion loss that SN75DPHY440SS can support?
Best regards,
Randy
Randy
Please reference to this table.
So max insertion loss DPHY440 can compensate at 1GHz (500MHz) is 4dB and at 1.5GHz (750MHz) is 5dB.
On the TX side, we have pre-emphasis that can provide 2.5dB compensation.
Thanks
David
Hi David,
This only describe D-PHY gen_1 and gen_2( 1 Gbps / 1.5 Gbps ), how about the insertion loss this IC can tolerate in D-PHY gen_3 speed?(2.5Gbps)
Thank you.
Luke
Luke
The DPHY440 does not support 2.5Gbps, therefore we do not need to specify the insertion loss at 2.5Gbps.
Thanks
David