Dear TI,
I am interested to use an DDI output from the intel GPU to a HDMI connector.
However, as I understand DDI is equivalent to DP++, is that right ?
So A DP126, is compatible with HDMI 1.4b, however I cannot find a solution that is suitable for HDMI 2.0 with DDI input.
What component should I use. The DP159 supports only HDMI inputs, right ?
Is that only a biasing issue ?