Part Number: TPD1E10B06
Hi
Let me ask you a question about "failure mode" of TPD1E10B06.
I asked you the same question the other day and I got the following answer then.
TVS0500: Failure mode - Interface forum - Interface - TI E2E support forums
"It can be a short or an open failure. They can also degrade if the stress is slightly above the absolute maximum ratings."
Though the answer was "It can be Short or Open", I do not understand well about the answer.
Because the device maybe connected to "power line", in that case, "Short" conditioin is not good situation.
And that case (power line connected), failure condition of the device must be "Open", I suppose...
I would like to ask your idea again about this.
Thank you for your support.
Best Regards,
Takumi