Other Parts Discussed in Thread: TFP401A-Q1, DS90C387, , SN65LVDS93A-Q1
Hello,
In our design, we re planning to use TFP401A-Q1 based DVI-D to LVDS converter (Dual channel Full HD). As the Serializer chip output levels are 3.3V, we could not directly interface with DS90C189-Q1 chip inputs. We did not use DS90C387 due to temperature range. Can we use DS90C189-Q1 with resistor divider on the input (2.2K), will it work? do you see any timing issue with RC effect at the input?
thank you,