This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
I want to use PN DS125BR401A in my new design and I have few questions:
1) can I work only with PORT B?
2)if only port B is working, the PORT A pins (in,out, EQA,DEMA) can left floating? if not how should i need to connect them?
3) what is the component longevity?
Hi Roei,
1) can I work only with PORT B?
Yes
2)if only port B is working, the PORT A pins (in,out, EQA,DEMA) can left floating? if not how should i need to connect them?
I recommend terminating the input pins with an AC coupling cap and 50 ohm resistor to ground to ensure nothing is detected on the channels. The output and EQ pins can be left floating. I recommend choosing any of these characterized combinations for the DEM pins.
3) what is the component longevity?
You can find longevity information in the quality and reliability report: https://www.ti.com/quality-reliability-packaging-download/report?opn=DS125BR401ANJYR
Best,
Lucas
thanks!
by lonevity I ment, what is the manufacturing plan for this PN? there is a chance that he becomes obselete in the next few years?
Hi Roei,
As far as I know there's no plan to obsolete DS125BR401A and support for this part should continue for at least the next few years.
Best,
Lucas