Part Number: SN65HVS883


As shown in the figure, in order to reduce the brightness of diode D01, a current-limiting resistor R0 is connected in series. Please answer whether this connection affects the overall function of the circuit
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: SN65HVS883


As shown in the figure, in order to reduce the brightness of diode D01, a current-limiting resistor R0 is connected in series. Please answer whether this connection affects the overall function of the circuit
Hey Fenqiang,
It's currently a US holiday. One of our engineers will provide feedback tomorrow.
Thanks,
Rami
Hello Fenqiang,
The Resistor R0 will not affect the overall function of this circuit and will only affect the brightness of the diode. This is because the input stage at IP0(pin3) if used in a low-to-high transition the input signal will pass three internal signal checks and the new ouput signal will be available at the parallel input of the shift register, waiting to be latched in. At the same time this signal switches the output of the current limiter from ground to the RE-output to turn on the LED. Depeding on the value of your resistor will determine the brightness of your led.
Thanks and Regards,
Kameron