We want to control the "enable" pin of the power switch using the "PWRCTL3/BETEN" port.
However, there is no 3.3V output from the "PWRCTL3/BETEN" port.
Please see the following and help us.
1. schematic diagram
2. Current registers setting value
0x05 18
0x06 0F
0x07 8F
0x08 0F
0x0A 78
0x0B 80
0xF8 01
3. Issue
The voltage of "PWRON3_BATEN3" pin is 0V.
4. The value i want.
The voltage of "PWRON3_BATEN3" pin should be 3.3V.