Part Number: TPD4E05U06
Other Parts Discussed in Thread: TPD4E02B04
Hi Experts,
Cx is looking alternative for SP1004U-ULC-04UTG from Littelfuse, and sems TPD4E05U06 can be used.
Questions:
[1] TPD4E05U06 can be used as replacement? The functional block diagram is not exactly the same (diodes and TVS on TI, TVS only on littelfuse)? Are components equivalent?
[2] What is the meaning of straight-through/flow-through routing section 10.2.1, page 17/36, datasheet revN, February 2022) ? Does this mean that I "will/can/have to" solder/connect the NC pin to the signal pair trace?
[3] On the TI TPD4E05U06, I can see that there are Dn+ and Dn- pins, but, as the functional block diagram is totally symetrical, I feel that this is not imperative to connect "signal pair +" to Dn+. I can connect either signal to either pin, without taking into consideration the polarity. This Dn+/Dn- notation on the TI TPD4E05U06 is more confusing that useful?
[4] I wonder if the TPD4E02B04DQAR should not be a better choice (and a straight forward replacement of SP1004U-ULC-04UTG)?
Thank you.
Regards,
Archie A.