Part Number: ONET4201LD
Hello Team,
we are considering having two ONET4201 in parallel to increase the max current.
...not optimal from the jitter perspective that may come out, which may kill the signal.
On the other hand we have the option to calibrate the propagation delay out of measures and the FPGA can compensate for that.
Nevertheless the compensation/correction we can provide is limited but it can be done.
Do we have an indication on the input/output delay of the ONET4201LD over temperature range?
How does it change vs. temperature?
Just typical data is ok, so that we can understand if it can be accommodated or not.
Thanks,
SunSet