Other Parts Discussed in Thread: TCAN1057A-Q1
HI Team,
Just want to quick check if our CAN driver(e.g. TCAN1051-Q1) is voltage mode or current mode driver?
Thanks.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
HI Team,
Just want to quick check if our CAN driver(e.g. TCAN1051-Q1) is voltage mode or current mode driver?
Thanks.
Ted,
The newer device is TCAN1057A-Q1 in place of the TCAN1051-Q1.
I'm not 100% sure what you mean by the question. CAN drivers are differential drivers, but they are current-limited in the event of short-circuit events. You will see these described in the Electrical Characteristics as things like "differential output voltage" for different conditions, or as "short-circuit steady-state output current" for short/fault conditions.
Best,
Danny
HI Danny,
Is there a constant voltage source to drive the CANH/L output or a constant current source to drive CANH/L output?
Ted,
CAN drivers use GND and VCC as references when driving to create the differential signal, and the drivers are limited to 250 mA. In standard application it is uncommon to see the current limit come into play.
Best,
Danny