Part Number: DS92LV2422
Other Parts Discussed in Thread: DS90UB947-Q1
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: DS92LV2422
Other Parts Discussed in Thread: DS90UB947-Q1
Hi Santhosh,
What is the goal for this setup? Are you just looking for an LVDS SERDES setup from transmitting video?
For an LVDS setup, I would recommend looking at a DS90UB947 with a DS90UB948 setup, as this setup can take an LVDS input at the SER, and output LVDS at the deserializer.
With this setup, you can cover longer distances, passthrough display touch and interrupt data, and send a PWM though the GPIO.
As for cables and connectors over long distances, there are a few potential options and setups. Section 7.3.12.1 of the DS90UB948 datasheet details loss at certain cable lengths, how much loss the AEQ of the device can compensate for, as well as an example setup. Here are two pictures with our STP and coax recommendations:

Do you plan on generating a PWM from the serializer, or do you plan on passing one through?
Thanks,
Ryan
Hi Ryan Kitto,
Thank you so much for your suggestion.
Yes, I'm looking for an LVDS SERDES setup for transmitting video and all the associated signals.
Below image is the Display Connector Signal details that needs to be transmitted over a long distance.

I have following questions could you please help me.
1. Any suggestion for 5V/3.3V supply and backlight supply line transmission over longer distances without any loss?
2. What's the Part number of Single Lane/Link output in the DS90UB947-Q1 family.
3. Is there any alternative part if cost is a concern in the design.
4. Whether any signal condition circuitry/repeaters need to be placed in between for the long-distance transmission?
Thanks, help would be appreciated.
Santhosh
Hi Santhosh,
1.) We do recommend that a clean power supply providing power to device, but we do not have any guidance or suggestions for power over long distances.
2.) The DS90UB947 is capable of single lane FPD-LINK output, and the DS90UB948 is capable of single lane FPD-LINK input.
3.) If cost is a concern, you can look at the DS90UB925-Q1 and the DS90UB926-Q1. One thing to keep in mind is that these solutions may not have the same range as the DS90UB947-948.
4.) As far as I am aware, we do not have any guidance for longer transmissions. Our devices are generally spec'd at 15 meters, but quality of cables and channel spec can have an impact, causing it to go shorter or longer distances.
Additionally, I would like to note that I would recommend using an external generator for any PWM signals, as I believe our line of SERDES can only support PWM signal frequencies within the hundreds of Hz.
Please let me know if you have any other questions.
Thanks,
Ryan