Other Parts Discussed in Thread: TUSB542, HD3SS3212, HD3SS3220
Hi team,
I have a question from customer. Can you please advise on below?
I have a question regarding the USB3.0 hub and the USB-c connectors.
In the USB3.0 there are 3 differential pairs - D+ and D-; SSTX+ and SSTX-; SSRX+ and SSRX-. In the USB-C standard there are two more couples RX1; RX2; TX1; TX2. So if the USB-c connector is used for 3.0 operation is it accepted RX1+ and RX2+ to be shorted at the USB-C connector (the same for TX1- and TX2+/-)? This should allow plugging the USB cable in both directions washout necessity of additional multiplexing of the connections.
Thanks and regards,
Aida