This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Dear TI ,
HW : TI AM62x
I modify some device tree (k3-am62-main.dtsi , k3-am62x-sk-common.dtsi and k3-am625-skeleton.dts)
I run command as follows:
stty -F /dev/ttyS5 -echo -onlcr 115200
cat /dev/ttyS5 &
echo hello > /dev/ttyS5
I don't see any message. Please tell me how to modify device tree .
Hi Albert,
The dmesg log seems showing some pinmux are defined by multiple interfaces. Please review your device tree pinmux settings to ensure a PIN is only used by one interface.
And if any UART pin has mode0 in MMC pins, please disable the corresponding MMC interface in the device tree.
Dear Bin,
I modify as follows:
k3-am62-main.dtsi:
main_uart1: serial@2810000 {
compatible = "ti,am64-uart", "ti,am654-uart";
reg = <0x00 0x02810000 0x00 0x100>;
interrupts = <GIC_SPI 179 IRQ_TYPE_LEVEL_HIGH>;
power-domains = <&k3_pds 152 TI_SCI_PD_EXCLUSIVE>;
clocks = <&k3_clks 152 0>;
clock-names = "fclk";
main_uart1_pins_default: main-uart1-pins-default {
pinctrl-single,pins = <
AM62X_IOPAD(0x1ac, PIN_OUTPUT, 2) /* (E19) UART1_RXD */
AM62X_IOPAD(0x1b0, PIN_INPUT, 2) /* (A20) UART1_TXD */
>;
};
};
main_uart4: serial@2840000 {
compatible = "ti,am64-uart", "ti,am654-uart";
reg = <0x00 0x02840000 0x00 0x100>;
interrupts = <GIC_SPI 182 IRQ_TYPE_LEVEL_HIGH>;
power-domains = <&k3_pds 155 TI_SCI_PD_EXCLUSIVE>;
clocks = <&k3_clks 155 0>;
clock-names = "fclk";
main_uart4_pins_default: main-uart4-pins-default {
pinctrl-single,pins = <
AM62X_IOPAD(0x124, PIN_OUTPUT, 3) /* (A23) UART4_RXD */
AM62X_IOPAD(0x128, PIN_INPUT, 3) /* (B23) UART4_TXD */
>;
};
};
main_uart5: serial@2850000 {
compatible = "ti,am64-uart", "ti,am654-uart";
reg = <0x00 0x02850000 0x00 0x100>;
interrupts = <GIC_SPI 183 IRQ_TYPE_LEVEL_HIGH>;
power-domains = <&k3_pds 156 TI_SCI_PD_EXCLUSIVE>;
clocks = <&k3_clks 156 0>;
clock-names = "fclk";
main_uart5_pins_default: main-uart5-pins-default {
pinctrl-single,pins = <
AM62X_IOPAD(0x108, PIN_OUTPUT, 3) /* (D24) UART5_RXD */
AM62X_IOPAD(0x10C, PIN_INPUT, 3) /* (E23) UART5_TXD */
>;
};
};
main_uart6: serial@2860000 {
compatible = "ti,am64-uart", "ti,am654-uart";
reg = <0x00 0x02860000 0x00 0x100>;
interrupts = <GIC_SPI 184 IRQ_TYPE_LEVEL_HIGH>;
power-domains = <&k3_pds 158 TI_SCI_PD_EXCLUSIVE>;
clocks = <&k3_clks 158 0>;
clock-names = "fclk";
main_uart6_pins_default: main-uart6-pins-default {
pinctrl-single,pins = <
AM62X_IOPAD(0x118, PIN_OUTPUT, 3) /* (D25) UART6_RXD */
AM62X_IOPAD(0x120, PIN_INPUT, 3) /* (C24) UART6_TXD */
>;
};
};
/*
sdhci2: mmc@fa20000 {
compatible = "ti,am62-sdhci";
reg = <0x00 0xfa20000 0x00 0x260>, <0x00 0xfa28000 0x00 0x134>;
interrupts = <GIC_SPI 82 IRQ_TYPE_LEVEL_HIGH>;
power-domains = <&k3_pds 184 TI_SCI_PD_EXCLUSIVE>;
clocks = <&k3_clks 184 5>, <&k3_clks 184 6>;
clock-names = "clk_ahb", "clk_xin";
ti,trm-icp = <0x2>;
ti,otap-del-sel-legacy = <0x8>;
ti,otap-del-sel-sd-hs = <0x0>;
ti,otap-del-sel-sdr12 = <0x0>;
ti,otap-del-sel-sdr25 = <0x0>;
ti,otap-del-sel-sdr50 = <0x8>;
ti,otap-del-sel-sdr104 = <0x7>;
ti,otap-del-sel-ddr50 = <0x8>;
ti,itap-del-sel-legacy = <0xa>;
ti,itap-del-sel-sd-hs = <0xa>;
ti,itap-del-sel-sdr12 = <0xA>;
ti,itap-del-sel-sdr25 = <0x1>;
ti,clkbuf-sel = <0x7>;
};
*/
test result:
Please help fix this issue .
I modify the device tree again.
k3-am625-skeleton.dts:
&main_pmx0 {
main_uart0_pins_default: main-uart0-pins-default {
pinctrl-single,pins = <
AM62X_IOPAD(0x1c8, PIN_INPUT, 0) /* (D14) UART0_RXD */
AM62X_IOPAD(0x1cc, PIN_OUTPUT, 0) /* (E14) UART0_TXD */
>;
};
main_uart1_pins_default: main-uart1-pins-default {
pinctrl-single,pins = <
AM62X_IOPAD(0x1ac, PIN_OUTPUT, 2) /* (E19) UART1_RXD */
AM62X_IOPAD(0x1b0, PIN_INPUT, 2) /* (A20) UART1_TXD */
>;
};
main_uart4_pins_default: main-uart4-pins-default {
pinctrl-single,pins = <
AM62X_IOPAD(0x124, PIN_OUTPUT, 3) /* (A23) UART4_RXD */
AM62X_IOPAD(0x128, PIN_INPUT, 3) /* (B23) UART4_TXD */
>;
};
main_uart5_pins_default: main-uart5-pins-default {
pinctrl-single,pins = <
AM62X_IOPAD(0x108, PIN_OUTPUT, 3) /* (D24) UART5_RXD */
AM62X_IOPAD(0x10C, PIN_INPUT, 3) /* (E23) UART5_TXD */
>;
};
main_uart6_pins_default: main-uart6-pins-default {
pinctrl-single,pins = <
AM62X_IOPAD(0x118, PIN_OUTPUT, 3) /* (D25) UART6_RXD */
AM62X_IOPAD(0x120, PIN_INPUT, 3) /* (C24) UART6_TXD */
>;
};
};
k3-am62-main.dtsi:
/*
sdhci2: mmc@fa20000 {
compatible = "ti,am62-sdhci";
reg = <0x00 0xfa20000 0x00 0x260>, <0x00 0xfa28000 0x00 0x134>;
interrupts = <GIC_SPI 82 IRQ_TYPE_LEVEL_HIGH>;
power-domains = <&k3_pds 184 TI_SCI_PD_EXCLUSIVE>;
clocks = <&k3_clks 184 5>, <&k3_clks 184 6>;
clock-names = "clk_ahb", "clk_xin";
ti,trm-icp = <0x2>;
ti,otap-del-sel-legacy = <0x8>;
ti,otap-del-sel-sd-hs = <0x0>;
ti,otap-del-sel-sdr12 = <0x0>;
ti,otap-del-sel-sdr25 = <0x0>;
ti,otap-del-sel-sdr50 = <0x8>;
ti,otap-del-sel-sdr104 = <0x7>;
ti,otap-del-sel-ddr50 = <0x8>;
ti,itap-del-sel-legacy = <0xa>;
ti,itap-del-sel-sd-hs = <0xa>;
ti,itap-del-sel-sdr12 = <0xA>;
ti,itap-del-sel-sdr25 = <0x1>;
ti,clkbuf-sel = <0x7>;
};
*/
dmesg | grep serial
echo hello > /dev/ttyS1 . It can't show any message .
Please help fix this issue .
Dear Bin,
About /dev/ttyS1, run echo hello > /dev/ttyS1 command . Measure UARt1_TXD , there is waveform output . But Measure UARt1_RXD , there is not waveform output . UART1_TXD and UART1_RXD is connected .
Please check if my tree is correct ?
k3-am625-skeleton.dts:
&main_pmx0 {
main_uart0_pins_default: main-uart0-pins-default {
pinctrl-single,pins = <
AM62X_IOPAD(0x1c8, PIN_INPUT, 0) /* (D14) UART0_RXD */
AM62X_IOPAD(0x1cc, PIN_OUTPUT, 0) /* (E14) UART0_TXD */
>;
};
main_uart1_pins_default: main-uart1-pins-default {
pinctrl-single,pins = <
AM62X_IOPAD(0x1ac, PIN_OUTPUT, 2) /* (E19) UART1_RXD */
AM62X_IOPAD(0x1b0, PIN_INPUT, 2) /* (A20) UART1_TXD */
>;
};
main_uart4_pins_default: main-uart4-pins-default {
pinctrl-single,pins = <
AM62X_IOPAD(0x124, PIN_OUTPUT, 3) /* (A23) UART4_RXD */
AM62X_IOPAD(0x128, PIN_INPUT, 3) /* (B23) UART4_TXD */
>;
};
main_uart5_pins_default: main-uart5-pins-default {
pinctrl-single,pins = <
AM62X_IOPAD(0x108, PIN_OUTPUT, 3) /* (D24) UART5_RXD */
AM62X_IOPAD(0x10C, PIN_INPUT, 3) /* (E23) UART5_TXD */
>;
};
main_uart6_pins_default: main-uart6-pins-default {
pinctrl-single,pins = <
AM62X_IOPAD(0x118, PIN_OUTPUT, 3) /* (D25) UART6_RXD */
AM62X_IOPAD(0x120, PIN_INPUT, 3) /* (C24) UART6_TXD */
>;
};
};