Part Number: TCAN1167-Q1
Other Parts Discussed in Thread: TCAN1044-Q1
We need IBIS Model for this device TCAN1167DMTRQ1 for Signal Integrity simulation between microcontroller and this CAN.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TCAN1167-Q1
Other Parts Discussed in Thread: TCAN1044-Q1
We need IBIS Model for this device TCAN1167DMTRQ1 for Signal Integrity simulation between microcontroller and this CAN.
Shanjai,
Whenever TI creates IBIS models for particular components, you will find it linked in the product folder under the "Design & Development" section. For the TCAN1167-Q1 we don't have a specific IBIS model under that name.
For the purposes of your simulation, you could use the IBIS model for the TCAN1044-Q1. This is document SLLM495 on the TCAN1044-Q1 product folder or linked HERE for your convenience.
Best,
Danny
Dear Danny,
The package of TCAN1167DMTRQ1 is VSON (14). But, IBIS model of TCAN1044-Q1 has the package of SOIC-D (8). Do they have different package lead inductance? And also please confirm do they have same I/O buffer model?
Please explain my query.
Shanjai,
The reason I'm pointing to the TCAN1044-Q1 is because the CAN transceiver is fundamentally the same, however you are correct, the model serves as a guide rather than an exact replica of its performance. Most modeling projects have the goal of seeing the approximate behavior of CANH/CANL on a bus. There is not an IBIS model specifically for TCAN1167-Q1, but the TCAN1044-Q1 model can serve to help with your design goals.
The logic I/O pins are similar for the devices as well.
Best,
Danny
Dear Danny,
The device TCAN1167DMTRQ1 has SPI clock, chip select, SDI and SDO. But in TCAN1044-Q1 does not have SPI communication pins. Could please suggest a solution to simulate SPI lines between MCU and CAN SBC?
Could you please support me as soon as possible?
Shanjai,
There is no such model that will simulate actual SPI communication between the TCAN1167-Q1 and a microcontroller. There is rarely a need to simulate SPI communication via IBIS. Unfortunately there are no IBIS models available that will simulate SPI communication from this transceiver. The IBIS models that exist serve the purpose of signal integrity evaluation on the bus, as this is where the majority of signal reliability considerations exist.
Best,
Danny