Part Number: TCAN4551-Q1
Hello team,
My customer has 4 questions on the nWKRQ pin.
1. Is there any timing chart when 16'h0800[8] = 1? On the datasheet, it seems that the timing chart represents when 16'h0800[8] = 0 as the nWKRQ is related to INH state.
2. Is it going to be asserted to LOW when wake event is occured?
3. Is my understanding below about 16'h0800[19] correct?
0 = nWKRQ is going to be operated by internal 3.6V rail with push-pull output.
1 = nWKRQ is going to be operated by external VIO voltage with Open drain output.

4. Is internal 3.6V going to be active, under consdition of VSUP: ON and VIO: OFF? The customer is planning to use nWKRQ as the WAKE signal with VIO.
Best Regards,
Kei Kuwahara