Part Number: TUSB1002
Hi team,
The TUSB1002RGET (USB3.1 linear driver) has a symptom of USB disconnection when a quenching agent is used.
In this device, when operated at low temperatures, the following symptoms were observed
Degradation of signal waveforms (smaller amplitude)
The port potential of the Floating hardware setting pin changes, and the setting dynamically switches during operation.
Do problems such as the following occur?
Sincerely.
Ryu