Other Parts Discussed in Thread: DS250DF210, DS250DF810, DS280DF810, DS250DF230
Hi team,
We are considering DS250DF410ABMR for a 24.33024Gbps interface due to the length of the PCB trace in the board(~23inches)(See Ref#1). While comparing DS250DF230 with DS250DF410, we have noticed that this datarate is specifically mentioned as one of the standard datarate in datasheet(see Ref#2 below). But, in DS250DF410 datasheet, the same is not mentioned and only a range ≥ 20.6 Gbps to ≤ 25.8 Gbps is specified(see Ref#3 below).
Additionally, in DS2x0DFxx0_SNLU182G_Programmers_Guide, the subrate mentioned as standard ones for DS250DF410 does not include 24.33024 Gbps(Table 7-6. DS280DF810, DS250DF810, DS250DF410, DS250DF210 Standard Rate Modes Configurable from Reg_0x2F). It is also mentioned that we can manually set datarate, if the range is within the VCO range(see Ref#4 below).
Queries:
1) Can we use DS250DF410 for the 24.33024 Gbps? Do we need to take care of anything in particular(configuration, CAL_CLK etc..) for doing so?
2) Any comments on the block diagram shown in Ref#1?
3) Is it preferred to go with 2 qty of DS250DF410(as shown in Ref#1) or 3qty of DS250DF230 with 30.72MHz CAL_CLK(as shown in Ref#5) for this application? Please check and comment on Block diagram shown in Ref#5 as well. Let me know your thoughts.
Ref#1: Implementation block diagram
Ref#2: DS250DF230 datasheet mentioning about 24.33024Gbps support
Ref#3: Supported Datarate table in DS250DF410 datasheet
Ref#4: Manual datarate settings section in the DS2x0DFxx0_SNLU182G_Programmers_Guide
Ref#5: Implementation Block diagram with DS250DF230