Hello, team
We use 948 as the deserializer for the car's IVI display; When we touch the IVI screen, the turetouch IC data will be uploaded to the MCU through the IIC signal, and then the data will be filtered and transmitted back to the SOC of the host through 948-947; When we set the Mode_ SEL1 is set to 20Mbps/STP, it is found that some touch data between MCU and 948 will be lost; When the mode_sel1 set to 5Mbps/STP, it will not occur;
My question is:
1. How to calculate and select this 5Mbps or 20Mbps speed change to ensure it does not affect my current design?
2. Is there any other impact of back channel rate change, such as the video signals of forward channel ?
thanks!