Other Parts Discussed in Thread: DP83TC811S-Q1, DP83TD510E, DP83TG720R-Q1
Hi,
I need your assistance on finding the right Ti ethernet PHY for our next project.
Since the implementation is in Avionics ie. it is on plane. The copper cable wight is significant measure and I thought of the single pair as solution.
Here are the parameters needed :
Single pair Ethernet PHY for copper cable connection.
Speed 100M
Guarantied Distance 90m (100 and above is ok)
The temperature rating should be 125C
Mac interface RMII or SMII
I have looked on several PHYs but was not sure about the cable length the PHY guarantee to work. The following PHYs:
- DP83TC811S-Q1 100BASE-T1 – IEEE 802.3bw Compliant from what I understand the distance here is 15m
- DP83TD510E which is 802.3cg 10Base-T1L 10M BPS but can it operate at 100M BPS @90 meters ?
- DP83TG720R-Q1 which is for 1G BPS IEEE802.3bp 1000BASE-T1 compliant. But will be the distance when operated in 100M bps ?
Where can I find the test over distance done foe the specific PHY? I did not see any mentioning of distance in the data sheet .
I will appreciate if you can share the PHY road map if there is no current PHY that support my requirements and will be in near future. (can be done by TI Israel if it is classified)
Thanks,
Avner