Other Parts Discussed in Thread: DS90C189-Q1, SN65LVDS93B-Q1
Hi Team,
The function of DS90C387 is not enough, is there a new generation product?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Team,
The function of DS90C387 is not enough, is there a new generation product?
Hello Kevin,
Can you be more specific about what function is not enough on DS90C387?
Best Regards,
Casey
Hi Team,
Need suggest alternative that can meet TA -40 degrees to above 85 degrees.
Kevin,
We don't have a device with the same functionality at DS90C387 that can meet -40 to 85C temp range, but we may have a similar alternative depending on what your use case is.
Do you need 48 pin inputs to dual LVDS output specifically (dual 24 bit color mode)? Or are you using the DS90C387 in 24 bit color mode (24 inputs to dual LVDS output)?
If you are using 24 bit color mode, then a device like DS90C189-Q1 would be a suitable alternative since it can support up the temp and range and similar PCLK rates with 24 bit input to dual LVDS output.
If you are using dual 24 bit color mode, then maybe a combination of two devices would be viable? For example 2x SN65LVDS93B-Q1?
Best Regards,
Casey