Part Number: DS90UB936-Q1
Other Parts Discussed in Thread: DS90UB953-Q1EVM, DS90UB933-Q1, , ALP
Hi
I'm trying to get a pattern generated from DS90UB953-Q1EVM.
I'm using a driver for ds90ub936-q1 for a camera that uses ds90ub933-q1 as an example.
I was able to detect the EVM address and set the back channel speed to 50 Mbps, and with this the serializer is detectable. But I am unable to get the pattern from the other side.
For a camera, the init sequence is the following:
WriteI2C(0x4c, 0xf)
WriteI2C(0x5b, 0xb0)
WriteI2C(0x5d, 0x48)
WriteI2C(0x4c, 0x1)
WriteI2C(0x5b, 0xb0)
WriteI2C(0x5c, 0xb0)
WriteI2C(0x5d, 0x48)
WriteI2C(0x65, 0x48)
WriteI2C(0x7c, 0x81)
WriteI2C(0x72, 0x0)
WriteI2C(0x70, 0x1e)
WriteI2C(0x6d, 0x7f)
WriteI2C(0xc, 0x3)
Most of this settings is to write the I2C address is expecting, however since I'm trying to use the pattern generation feature, I don't have a sensor. What should I write to registers 0x5d and 0x5e?
Thanks in advance,
Leonardo