Hello guys,
One of my customers is considering using DP83825I for their new products.
At this moment, they have the following questions.
Could you please give me your reply?
Q1.
What voltage node is RST_N terminal internal pull up connected to?
Q2.
If the answer for Q1 is 3.3V, is it no problem because the device datasheet says RESET pin recommended operation condition is VDDIO+/-10%.(VDDIO=1.8V) on page 5, 6.3 Recommended Operating Conditions section.
Q3.
This is question regarding to Q2.
What is VDDIO voltage of RESET recommended voltage range? Is it 1.62V~1.98V? Or 3V~3.6V?
Your reply would be much appriciated.
Thank you and best regards,
Kazuya.